The Smarter Approach

Safer and sustainable operations with data-enabled docking and mooring equipment

Nov 04, 2021

Balancing port safety, efficiency, sustainability and investment costs to accommodate the future of the shipping industry, has become a consistent challenge.

Read more

Trelleborg Publishes Expert Opinion Piece On The Docking And Mooring Challenges Facing Today’s Ports

Dec 22, 2020

Trelleborg Marine and Infrastructure has published an informative expert opinion piece, titled ‘A Balancing Act’, which is based on discussions with key individuals on the front line of port operations. Now available online for download, it focuses on the docking and mooring challenges facing today’s port environments and how port and maritime consultants are responding to optimize windows of operation.

Read more

Trelleborg Hosts Three-Part Smarter Approach Webinar Series

Nov 10, 2020

Trelleborg’s marine and infrastructure operation in the US recently held an educational three-part webinar series for close to 60 Moffatt & Nichol engineers and consultants. Designed to arm delegates with experience-based knowledge, the webinars covered Marine Fender, Docking and Mooring equipment, Ship-Shore Links and Navigation and Piloting solutions design and specification best practice.

Read more

Reducing the Effects of Passing Ships

Feb 24, 2020

Throughout the world, ports are continually facing the challenge of maintaining and increasing productivity. Vessel berth utilization and availability are keys that govern product or passenger transfers to occur as effectively as possible.

Read more

LNG Transfer: Strengthening the Chain Of Custody With Integrated Monitoring

Feb 18, 2020

Last year, we saw the LNG shipping sector hit new heights. LNG carrier orders were strong; in February 2019, according to Cleaves Securities, the LNG orderbook stood at a record high, with ship owners planning to order as many as 69 LNGCs, up from 65 in 2018 and only 17 in 2017.

Read more

Safe LNG Transfer and the Revision of the EN 1474-2 Standard

Feb 11, 2020

Ever since the International Maritime Organization first agreed to limit the sulphur content in all marine fuels to 0.5 percent beginning in 2020, we’ve seen a substantial rise in the demand for LNG bunkering infrastructure. Now that we have arrived in 2020, we’re sensing a real urgency is permeating the industry, as ports and ship owners alike ensure that they are compliant.

Read more

Port of Tallinn to optimize mooring with Trelleborg's AutoMoor

Aug 13, 2019

Docking and mooring plays a critical role in increasing throughput of an individual berth and overall port facility. No matter the application, ports and terminals worldwide are under pressure to increase throughput. However, trying to do so at the same time as dealing with increasing vessel sizes can be challenging.

Read more

Trelleborg to supply smart rope free mooring system to Port of Langnas

Feb 20, 2019

Discover how port automation is to increase reliability, safety and efficiency at The Port of Langnas.

Read more